{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the impedance value of the input line reactor modification X07 on the S-Flex enclosed drives?
Issue:
Impedance value of the input line reactor modification X07 on the S-Flex enclosed drives.

Product Line:
Altivar Machines, S-Flex

Environment:
All S-Flex

Cause:
Needs to know the input line impedance for the X07 input line reactor mod on the S-flex enclosed drives.

Resolution:
The impedance value for the input line reactor X07 mod is 1.5%

Schneider Electric Global