Issue:
Max and Min for deceleration on an ATS22.
Product Line:
Altistart 22
Resolution:
It ranges from freewheel stop (default) or from 1 to 60 seconds. This "dEC" parameter can be found in the "SEt" menu.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global