undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the purpose of the external battery of the M221?
1) The help content give us the information the battery of the M221 allow:
-to save the content of the whole %MW area ( %MWi  with i>50;  note: %MW0-%MW49 are also save without battery)
- to save the RTC clock

2) But in reality the battery is always needed/mandatory because without battery the PLC can’t start in RUN after a PowerOFF, PowerON of the PLC
Within %S75 the PLC program can check when the battery has the be replaced before it become out of order  (in average every 4/5 years):

When this bit is Set to 1, it means external battery power is low, so has to be replaced soon

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: