Issue:
What is the "EPSS_DataCollector" SQL account password?
Product Line:
Power Monitoring Expert 7.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020 (9.1)
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024
Environment:
Fresh Install of Power Monitoring Expert
Cause:
What is the "EPSS_DataCollector" SQL account password?
Resolution:
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*
The password for the SQL account "EPSS_DataCollector" created during PMEDC/PMEHC installer is PASSWORD_1234
In order to change this password, in addition to updating it in SQL Server Management Studio, the following file needs to be updated with the new password:
...\Schneider Electric\Power Monitoring Expert\Data Collector\Web.config
Search for "EPSS_DataCollector" and replace the password field with the new password in three locations.
For versions of PME past 9.0, the EPSS collector user has been integrated as a role for the ION and ionedesd users. Ticking the field here will enable access for the Web Apps.
Released for: Schneider Electric Global