{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Variables limitation using recipeDB service
Issue

Web Designer help mentions that 1000 variables can be use in a projects, however this doesn’t apply when the RecipeDb service is used with an automatic request.

Product Line

Factory cast HMI (WMY, NMW)


Resolution

When using an automatic request with the recipeDB, the maximum number of variables (integers) should be limited to 300 to insure the stability of the Tsxwmy100.

Schneider Electric Global