{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the center dividing section of the NetShelter SX Colocation be removed?
Issue:
Customers may want to remove the center divider in the NetShelter SX Colocation cabinet.

Product Line:
NetShelter SX Colocation

Environment:
All versions and serial ranges.

Cause:
For various reasons, including the want to mount a particular 0U PDU, customers may wish to remove the center divider of the cabinet.

Resolution:
The center divider of the NetShelter SX Colocation cabinet is not user removable. The divider separates the two sections of the cabinet for security purposes so it's not removable.

Schneider Electric Global