Issue:
Customer wants to know the temperature and altitude limitations for the ATV32/ATV320 drive.
Product line:
ATV32, Altivar 32, ATV320, Altivar 320
Environment:
All
Cause:
n/a
Resolution:
The voltage range for the M2 drives (200-240V) is 200V, minus 15% to 240V, plus 10%.
The voltage range for the N4 drives (380-480V) is 380V, minus 15% to 480V, plus 15%.
The temperature rating for all models is +14F to +122F (-10C to +50C), without derating (as long as the switching frequency is 4 kHz or less).
Optional derating is available from +122F to +140F (50C to 60C). Consult the Installation manual for de-rating curves based on the temperature and switching frequency.
The maximum altitude the Altivar 32 can be installed without de-rating is up to 3300 feet (1000 meters). De-rate the drive nominal current by each additional 330 feet (100m) up to a maximum ceiling of 10,000 feet (3000m).
Customer wants to know the temperature and altitude limitations for the ATV32/ATV320 drive.
Product line:
ATV32, Altivar 32, ATV320, Altivar 320
Environment:
All
Cause:
n/a
Resolution:
The voltage range for the M2 drives (200-240V) is 200V, minus 15% to 240V, plus 10%.
The voltage range for the N4 drives (380-480V) is 380V, minus 15% to 480V, plus 15%.
The temperature rating for all models is +14F to +122F (-10C to +50C), without derating (as long as the switching frequency is 4 kHz or less).
Optional derating is available from +122F to +140F (50C to 60C). Consult the Installation manual for de-rating curves based on the temperature and switching frequency.
The maximum altitude the Altivar 32 can be installed without de-rating is up to 3300 feet (1000 meters). De-rate the drive nominal current by each additional 330 feet (100m) up to a maximum ceiling of 10,000 feet (3000m).
Released for:Schneider Electric Global