{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the Adapter Plate that is used to replace the ATV58 with the ATV61/71 be used when converting the Flex58 to the ATV61/71?
Issue:
Converting the Flex58 to the ATV61/71 using Adapter plate?

Product Line:
ATV61 and ATV71

Environment:
Frame size 2 to frame size 8

Cause:
Converting from the ATV58/FLEX58 to the ATV61/71

Resolution:
The Adapter plate that is used for mounting the ATV61/ATV71 in the same foot print as the ATV58 cannot be used to replace the FLEX58 with the ATV61/71 . The foot print of the FLEX58 is different from that of the ATV58, this difference is not compatible with the mounting plate.

Schneider Electric Global