{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the Altivar ATV312 Drives do single phase 110 VAC input?

Issue:
ATV312 single phase 110 VAC input

Product Line:
ATV312 Drives

Environment:
All serial numbers for ATV312 Drives

Cause:
N/A

Resolution:
No it cannot. The drive can only do 208/230 VAC single-phase on the single phase input rated drives that have the M2 suffix..

Schneider Electric Global