{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
I cannot connect to the M580 CPU with Unity Loader
By default, the M580 CPU's ftp service is disabled (preferred option for cyber security ).
Unity Loader will not connect if it cannot establish connection to ftp.
To enable ftp on your CPU (with SV<=3.20), load an application into the CPU, that has FTP enabled. You can enable in Control-Expert in the Security Tab of the  ethernet ports configuration of the M580 CPU :
capture