Issue:
Customers want to know the cfm rating of NetShelter CX cabinets with the AR4703 fan booster installed.
Product Line:
NetShelter CX.
Environment:
All versions and serial ranges.
Cause:
Installing the AR4703 increases the cfm of the NetShelter CX cabinet.
Resolution:
18U with 1x AR4703 - 260 CFM
24U with 2x AR4703 - 330 CFM
38U with 3x AR4703 - 340 CFM
Customers want to know the cfm rating of NetShelter CX cabinets with the AR4703 fan booster installed.
Product Line:
NetShelter CX.
Environment:
All versions and serial ranges.
Cause:
Installing the AR4703 increases the cfm of the NetShelter CX cabinet.
Resolution:
18U with 1x AR4703 - 260 CFM
24U with 2x AR4703 - 330 CFM
38U with 3x AR4703 - 340 CFM
Released for:Schneider Electric Global