{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can you use a TM3 module with a Twido programmable controller or an OTB distributed IO system?
Issue:
Use of TM3 modules with Twido or OTB.

Product line:
Twido, OTB and TM3 I/O

Environment:
TwidoSoft and TwidoSuite

Cause:
Modules not being seen in pick list  or added in and not being detected.

Resolution:
No, you cannot use a TM3 module with a Twido programmable controller or an OTB distributed IO system, only TM2 or TWD modules can be used.