Issue:
I/O scanning health bit address for a M340 NOE module.
Product Line:
M340 PLC
Resolution:
If a BMX NOE 01x0 module is configured in rack 0, slot 3, the health bit address would be as follow:
%IW0.3.0.1 device 1 - 15
%IW0.3.0.2 device 16 - 31
%IW0.3.0.3 device 32 - 47
%IW0.3.0.4 device 48 - 64
I/O scanning health bit address for a M340 NOE module.
Product Line:
M340 PLC
Resolution:
If a BMX NOE 01x0 module is configured in rack 0, slot 3, the health bit address would be as follow:
%IW0.3.0.1 device 1 - 15
%IW0.3.0.2 device 16 - 31
%IW0.3.0.3 device 32 - 47
%IW0.3.0.4 device 48 - 64
Released for:Schneider Electric Global