{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the screen resolutions that are supported under Generic PC Runtime in Vijeo Designer v6.2?
Issue:
What are the screen resolutions that are supported under Vijeo Designer Generic Windows PC Runtime?

Product Line:
Screen resolution, 4:3, 16:9, aspect ratio, 1080p, 1080i, 720p

Environment:
Generic Windows PC Runtime, Vijeo Designer

Resolution:
Below are the list of display resolutions available for the generic PC runtime:
800 x 600 (SVGA)
1024 x 768 (XGA)
1280 x 720 (HD720)
1280 x 1028 (WXGA)
1366 x 768 (FWXGA)
1440 x 900 (WSXGA)
1600 x 1200 (UXGA)
1680 x 1050 (WSXGA+)
1920 x 1080 (HD1080)
1920 x 1200 (WUXGA)
2560 x 1600 (WQXGA)

Keep in mind that the limitation of the resolution usually depends on the graphics chip on the industrial PC and monitor that are used.