Issue:
Is it possible to run an ATS22 with a smaller motor or without a motor attached?
Product Line:
Altistart ATS22
Environment:
All models
Cause:
Need for testing starter with minimal or no load attached.
Resolution:
No. SSt is a feature of the ATS48 soft start. It is not available on the ATS22.
It has to have a load at the output.
The following video is a tutorial for understanding the Small-Load or No-Motor limitations of Altistart 22:
Is it possible to run an ATS22 with a smaller motor or without a motor attached?
Product Line:
Altistart ATS22
Environment:
All models
Cause:
Need for testing starter with minimal or no load attached.
Resolution:
No. SSt is a feature of the ATS48 soft start. It is not available on the ATS22.
It has to have a load at the output.
The following video is a tutorial for understanding the Small-Load or No-Motor limitations of Altistart 22:
Released for:Schneider Electric Global