Issue:
ATV212 configuration to do an automatic restart after power loss in local control
Product Line:
Altivar ATV212
Environment:
All
Cause:
Running the drive in local mode they need to have the drive restart in the event of loss of power.
Resolution:
The drive can not be programmed to do a automatic restart in local mode. You will need to push the start button again on the face of the drive to start the drive back up.
If you want a automatic restart after power loss consider using 2 wire terminal control instead.
ATV212 configuration to do an automatic restart after power loss in local control
Product Line:
Altivar ATV212
Environment:
All
Cause:
Running the drive in local mode they need to have the drive restart in the event of loss of power.
Resolution:
The drive can not be programmed to do a automatic restart in local mode. You will need to push the start button again on the face of the drive to start the drive back up.
If you want a automatic restart after power loss consider using 2 wire terminal control instead.
Released for:Schneider Electric Global