{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What fuse size is needed for the ATS22 CL1 CL2 control circuit?

Issue:
Looking for the fuse size needed for CL1-CL2 on ATS22 soft starts

Product line:
ATS22, Altistart 22

Environment:
All models (S6 and S6U)

Cause:
The drawings and installation show fuse/overcurrent protection on CL1, but no notes on what size or type of protection to use.

Resolution:
The CL1 - CL2 control voltage input should have a 1A fast acting fuse, or 1A circuit breaker for each ATS22 unit.  This applies to the 120V and 230V control supplies (Q, S6 and S6U).

fusesubnote

Schneider Electric Global