undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What cables can be use to connect to a M221 from a PC over USB?
Issue:
Connecting to the M221

Product line:
M221 all controllers

Environment:
EcoStruxure Machine Expert Basic (formally known as SoMachine Basic)

Cause:
Connection issues

Resolution:
The programming cables that can be used to connect to a M221 over USB are the following;
TCSXCNAMUM3P or the BMXXCAUSBH045.

Schneider Electric Global