{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How do I change the IP address of a Momentum M1E that has all ready been saved to flash?

If an IP address has been saved to the flash memory in the M1E processor then all you have to do is open the Concept project that was downloaded into the M1E and edit the configuration off-line. Change the IP address settings in the Extension or Ethernet I/O scanner pages then connect to the controller with the old IP Download and save the new configuration to flash, go off line and power cycle.

If you do not know the currently saved IP address then you can use Wireshark which is a free downloadable software at www.wireshark.org to find the lost IP address. Once you find the lost IP address then connect with Concept and download and flash the new Concept project as described above.

Schneider Electric Global