Issue:
Conduit kit for ATV12
Product Line:
ATV12, Altivar 12 Machine drive
Resolution:
The ATV12 drives do not have a NEMA 1 conduit kit option available. The drive will need to be mounted inside a separate enclosure.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global