{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to determine which option cards are installed on the ATV61 and 71 VFDs?
Issue:
Which option cards are installed on the ATV61 and 71 VFDs?

Product Line:
ALTIVAR 61, ALTIVAR 71,

Environment:
All drives all serial number

Cause:
N/A

Resolution :
To verify what options cards are installed on the Altivar 61 or the Altivar 71 VFD you can do the following:
Drive menu - Press enter
Identification Sub Menu -  Press enter
Scroll to Option 1 and Option 2, there the two options will display the option cards installed on the VFDs

Schneider Electric Global