{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to transfer program from one ATV212 to another with different horsepower ratings using SoMove?
Issue:
Transfer program from ATV212 to an ATV212 with different horsepower ratings using SoMove?

Product Line:
Altivar 212, Altivar Machine

Environment:
All

Cause:
Copy programming between drives of different sizes.

Resolution:
No, it is not possible to transfer files between drives with different horsepower ratings.  The reference (part number of the drive) must match.

Schneider Electric Global