{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why do I get Diagnostic error code 0x000401 on a PM8ECC after I set a new IP address?
Issue:
After setting an IP address in the PM800's PM8ECC there appears a diagnostic error 0x000401.

Product Line:
PM800
PM8ECC

Environment:
PM800
PM8ECC

Cause:
Occurs when the PM8ECC has been programmed with a duplicate IP address.

Resolution:
Change the IP address to an IP that is not being used by another device.

Schneider Electric Global