{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How convert a 984 HSBY application to Unity
Issue
How convert a 984 HSBY application to Unity

Product Line
Unity

Environment
Windows 10

Resolution
  • Open the ProWORX 32 application.


  • Select the appropriate settings in the 'L984 Options' window.
  • Click on OK


  • The application imported without any errors.   Attempts to rebuild the application will fail with two errors:


This error is expected because the application contains a CHS loadable function block.

The reason for the error is because Unity is not able to delete the CHS loadable block.  The CHS block is not needed in a Unity
Hot Standby application.  The Hot Standby function is managed from Hot Standby window in the PLC configuration.

To resolve the issue:

  • Double click on the error message (This will open the DFB)

User-added image

  • Delete the structured text in the DFB block.

User-added image

  • Rebuild the application.
  • Save the changes.

Schneider Electric Global