Issue:
Can a SS be used on Wye start / Delta run type motor?
Product Line:
Altistart soft starters
Environment:
All models, All serial numbers
Cause:
Customer has an existing Wye/Delta motor but would like to connect a soft starter to it. They are unsure where to connect the soft start.
Resolution:
Yes, an ATS22 and ATS48 Soft Starter can be used on a Wye/Delta type motor. The output of the starter should be connected to the motor run windings only (usually the delta).
Can a SS be used on Wye start / Delta run type motor?
Product Line:
Altistart soft starters
Environment:
All models, All serial numbers
Cause:
Customer has an existing Wye/Delta motor but would like to connect a soft starter to it. They are unsure where to connect the soft start.
Resolution:
Yes, an ATS22 and ATS48 Soft Starter can be used on a Wye/Delta type motor. The output of the starter should be connected to the motor run windings only (usually the delta).
Released for:Schneider Electric Global