Issue Is there a way to restore the default username and password for the web page access to the M340 Ethernet module. Product Line M340 BMXNOExxx, BMXNOCxxx Environment Windows 10 version 1902, BMXP342020, BMXNOE0100 Resolution The user lost the password and cannot access the web pages in the M340 Ethernet module. They need tp restore the default username and password. The only way to restore the default username and password is to go into the M340 Ethernet module to delete a specific file. This requires using an internal proprietary username and password to access it. Due to security reasons, this username and password cannot be given out to either the customer or a Schneider Electric representative. In order to restore the default username and password, the M340 Ethernet module will need to be sent back for repair. |
Released for:Schneider Electric Global