{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you program the ATS22 softstarter to trip if it exceeds some number of starts per hour?
Issue:
How can ATS22 be programmed for a fixed number of starts per hour?

Product Line:
Altistart ATS22

Environment:
All

Cause:
Wants to delay the total number of times the softstarter can be started in one hour.


Resolution:
Programming:
Adj menu
Snb= number of starts  Off or 1 thru 10
SLG= Start period 1 min thru 60 mins

Example= if Snb= 3 and SLG is 10 mins   you can start and stop the drive 3 times in 10 mins.  If you exceed the programmed start time the drive will trip out on SnbF.

Schneider Electric Global

Attachment(s)
ats22_user_manual_en_bbv51330_02.pdf [3.02 MB]