Issue:
Can the ATV32 drive with Modbus Ethernet TCP/IP do token ring topology?
Product Line:
ATV32
Environment:
All models and serial numbers
Cause:
None
Resolution:
No, the token ring topology is not compatible with the ATV32 running Modbus Ethernet TCP/IP protocol. See the Modbus TCP Ethernet/IP Communication Manual S1A28701 for further details.