{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Legacy Factorycast Jave Bean applets does not work on the BMENOC0311
Issue
Legacy Factorycast Jave Bean applets does not work on the BMENOC0311

Product Line
BMENOC0311

Environment
Windows 10

Resolution
The LiveLabel and other Java Bean applets described in the help were used for the legacy 140NOE77110 Quantum Factorycast  modules. The applets are considered to be obsolete and we no longer have any Engineering support for it.  They are not intended to be used with the BMENOC0311.  It is recommended to use the Microsoft Expression Silverlight Factorycast objects when developing custom web pages for the BMENOC0311.

Schneider Electric Global