Issue:
Separate 120V control voltage needed to run an ATV312?
Product Line:
ATV312
Environment:
All
Cause:
Customer does not have 120VAC available
Resolution:
No. A separate 120Vac is not needed. Only line voltage is required.
When remote control is used, the VFD provides 24Vdc for the logic inputs.
Separate 120V control voltage needed to run an ATV312?
Product Line:
ATV312
Environment:
All
Cause:
Customer does not have 120VAC available
Resolution:
No. A separate 120Vac is not needed. Only line voltage is required.
When remote control is used, the VFD provides 24Vdc for the logic inputs.
Released for:Schneider Electric Global