{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to install Vijeo Designer as a silent install?
Issue:
Is it possible to install Vijeo Designer as a silent install?

Product Line:
Vijeo Designer

Environment:
Software installation on Windows PC

Resolution:
Yes, you can install Vijeo Designer as a silent install.  Below are the parameters that could be used for the install:
TypeDescriptionNotes
FIRSTNAME:
StringUser's first name
LASTNAME:
StringUser's last name
COMPANYNAME
StringUser's company name
REFERENCENUM
StringProduct Reference numberIf empty string, then the installer will use a pre-defined reference number
SERIALNUM
StringProduct Serial numberIf empty string, then the installer will use a pre-defined serial number
INSTALLDIR
StringInstallation path of Vijeo DesignerIf empty string, then the installer will use a pre-defined destination path
PROJECTSPATH
StringInstallation path of Vijeo Designer ProjectsIf empty string, then the installer will use a pre-defined projects path
STARTMENUPATH
StringStart Menu folder locationIf empty string, then the installer will use a pre-defined start menu folder path
DESKTOPSC
BooleanSpecifies to create a desktop shortcutIf the value is “true”, create a desktop shortcut. If “false”, do not create desktop shortcut
QUICKLAUNCHSC
BooleanSpecifies to create a quicklaunch shortcutIf the value is “true”, create a quick launch shortcut. If “false”, do not create a quick launch shortcut
INSTALLALLLANGS
BooleanSpecifies to install all application languagesWhen false, only the English language and help files are installed. If true, install all application languages and help files.
DEFAULTLANG
StringSpecifies default application languageIf empty string, then use language of locale. Possible values are ENU, CHS, DEU, FRA, ITA, ESP
ADMINRIGHTS
BooleanSpecifies to install as AdministratorIf “false”, install Vijeo Designer with for User Rights. If “true” installer Vijeo Designer for Administrator Rights
DEMO
BooleanSpecifies to install in Demo modeIf “true”, install Vijeo Designer in Demo mode. If “false”, install Vijeo Designer in Standard Mode.


































Below is an example on how the parameters above are used:
msiexec /i "C:\InstallerDirectory\Vijeo Designer 6.2.msi" FIRSTNAME="User" LASTNAME="User" COMPANYNAME="INDE Electronics" REFERENCENUM="VJDSNDTGSV62M" SERIALNUM="01234567890" INSTALLDIR="C:\Program Files\Schneider Electric\Vijeo Designer" DESKTOPSC="true" QUICKLAUNCHSC="true" ADMINRIGHTS="true" INSTALLALLLANGS="false" DEFAULTLANG="ENU" /qb

Where 62 in the REFERENCENUM="VJDSNDTGSV62M" signifies the version of Vijeo Designer you are installing.

Schneider Electric Global