{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How do I change the analog input AI2 on the ATV61 or ATV71 to accept 0-10Vdc instead of 4-20mA?

Article available in these languages: Finnish

Issue:
Changing the analog input AI2 on the ATV61 or ATV71 to accept 0-10Vdc instead of 4-20mA.

Product Line:
Altivar 61, Altivar 71

Environment:
All Serial Numbers

Cause:
Programming and wiring of an analog input AI2.

Resolution:
Go into Drive menu and then 1.5 Inputs/Outputs menu.
Go into AI2 submenu and change AI2 type to voltage.
Min and max values can be adjusted as needed.  Example would be min 0vdc and max 10vdc.



If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global