Issue
In Profile Editor, there are two PM5000 options, PM5000S and PM5000S1
Product
StruxureWare Power SCADA Expert (PSE) 7.4, 8,0, 8.1
PowerSCADA Operations (PSO) 8.2
Environment
Profile Editor
Resolution
Select the PM5000S profile to add a PM5560 device to a project.
In Profile Editor, there are two PM5000 options, PM5000S and PM5000S1
Product
StruxureWare Power SCADA Expert (PSE) 7.4, 8,0, 8.1
PowerSCADA Operations (PSO) 8.2
Environment
Profile Editor
Resolution
Select the PM5000S profile to add a PM5560 device to a project.
Released for:Schneider Electric Global