{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the changes on the Micrologic trip unit performance when we install a LT Off Rating Plug?
When you use the LR off plug that means Ir = 1 and Tr = very far from standard times delay (near infinity). There is a direct relationship between load shedding and the long time delay protection so for this reason the load shedding will remain off too. You can replace it with the 3 alarms called Ia max, Ib max and Ic max, each alarm have to work in relationship with 3 contacts of the M6C. The power shedding feature is not affected if you install a LT Off Rating Plug

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.