{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the maximum roof load rating for NetShelter SX and SV cabinets?
Issue:
Information regarding the maximum load rating for the roof is required

Product Line:
NetShelter SX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
The load rating should not be exceeded.

Resolution:
The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.