Issue
Unity shows the DTM version as 1.1.3.0 for the DTM that is installed using 'PRMMasterSetup.exe' version 1.1.4.0.
Product Line
TCSEGPA23F14F, M580, M340
Environment
TCSEGPA23F14F version 1.1.3.0
Resolution
After installing the Master DTM version 1.1.4.0, Unity shows the version of the DTM as 1.1.3.0.



The installation window and the Properties Details tab for the setup is incorrectly labeld as 1.1.4.0. It should be 1.1.3.0.
Unity shows the DTM version as 1.1.3.0 for the DTM that is installed using 'PRMMasterSetup.exe' version 1.1.4.0.
Product Line
TCSEGPA23F14F, M580, M340
Environment
TCSEGPA23F14F version 1.1.3.0
Resolution
After installing the Master DTM version 1.1.4.0, Unity shows the version of the DTM as 1.1.3.0.
The installation window and the Properties Details tab for the setup is incorrectly labeld as 1.1.4.0. It should be 1.1.3.0.
Released for:Schneider Electric Global