{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PME 7.2.2 database manager is giving a timeout error when performing archive or trim over a long time range
Issue:
While running a database archive, the archive or trim will fail with a 'timeout expired' error as shown below:



Running the archive or trim again over a much shorter time interval, such as an hour, will succeed.

Product Line:
Power Monitoring Expert 7.2.2

Environment:
Database Manager
Database Trim and Archive

Cause:
There were a number of timeout settings with Database Manager that were causing these issues. The timeouts were mainly a 30 second Trim timeout and an 18 hour archive timeout.

Resolution:
There is a hotfix available that will remove these timeout settings. In addition, the attached hotfix will also speed up the trim and archive process, without the unwanted side effects of a huge transaction log size increase and database tables locking up.

*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

To deploy the hotfix:
1. Rename databasearchive.dll and databasetrim.dll located in the ...\Power Monitoring Expert\system\bin folder to a different name
2. Copy in the new versions of these files to ...\Power Monitoring Expert\system\bin folder
3. In SQL Server Management Studio - run the scripts in the following order: PME7_ArchiveDBCopyDataLog.sql, then PME7_ArchiveDB_new.sql, then PME7_TrimRecords.sql.





Schneider Electric Global

Attachment(s)
PME7_TrimRecords.sql [4.24 KB]
databasearchive.dll [11.5 KB]
databasetrim.dll [5 KB]
PME7_ArchiveDB_new.sql [5.5 KB]
PME7_ArchiveDBCopyDataLog.sql [3.41 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.