Issue
How do I setup an HMIGTO to upload the program (.VDZ file) if needed to be later retrieved?
Product Line
Vijeo Designer
Environment
HMI Configuration Software
Resolution
1) Set the Data Location, "Data Files / Forms" to the desired storage location of the HMI:
Main Drive - uses the embedded memory
Secondary Drive is the SD Card or
Optional Drive - is the USB memory stick
2) Expand Download under the target properties.
3) Set the "Include Editor Project" checkbox to ticked.
4) Download the Vijeo Designer application to the HMI.
How do I setup an HMIGTO to upload the program (.VDZ file) if needed to be later retrieved?
Product Line
Vijeo Designer
Environment
HMI Configuration Software
Resolution
1) Set the Data Location, "Data Files / Forms" to the desired storage location of the HMI:
Main Drive - uses the embedded memory
Secondary Drive is the SD Card or
Optional Drive - is the USB memory stick
2) Expand Download under the target properties.
3) Set the "Include Editor Project" checkbox to ticked.
4) Download the Vijeo Designer application to the HMI.
Released for: Schneider Electric Global