{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ATV61/ATV71 input summing. With Reference channel set to HMI, does the MFR parameter reset to default (100%) after a power cycle?
Issue:
Input summing used in ATV61/ATV71, the HMI is being used for the multiplier input (MA2). MFR is being reset to 100% after each power cycle.

Product Line:
ATV61/ATV71

Environment:

All models, All serial numbers

Cause:
Information not available in current literature.

Resolution:
Yes, the MFR parameter will be reset to 100% each time power is cycled.  There is no way to save the value of MFR into EEPROM memory.  To prevent this from causing a problem, try using an analog input for your multiplier instead of the HMI.