undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Alternative for standard locking system for S3X enclosures with double door
For the installation of an alternative to the standard lock from S3X enclosures with double doors by a lock with another number of key. it is necessary to replace the escutcheon by the handle reference NSYMCSX. Example of DIN barrel usable on handle reference NSYMCSX - DIN barrel made by JMP Diffusion type 1327/999 - DIN barrel made by EMKA type 1109-U1-N See instruction sheet in attachment

Schneider Electric Global

Attachment(s)
Alternative for standard locking system for S3X enclosures with double door.pdf [169.29 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.