Issue:
Looking for assistance on how to connect the M340 PLC to a Magelis HMI in order to communicate over Modbus TCP/IP USB Equipment as defined in Vijeo Designer.
Product Line:
Vijeo Designer, Magelis HMI, M340
Resolution:
The BMX-XCA-USBH018 is the cable to communicate by Modbus TCP/IP via USB between the M340 and the HMIGTO5310.
The mini-USB end plugs into the M340 and the standard USB end plugs into the HMIGTO
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Global