{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can we deliver the medium power transformers completely without oil?
Yes, this is possible for Medium Power Transformers, however it's recommended to keep the transformer without filling the oil for a maximum of 6 months period. For cases where the transformer will be stored more than 6 months we recommend to dispatch the transformer with oil inside.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.