{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the difference of H class and F class in Tricast cast resin dry type transformers ?
The main difference is that the class designations refer to the withstand temperature of the insulation material in Tricast cast resin dry type transformers. Thus, H class has a wihstand temperature level of 180 ⁰C for the coils and F class of 155 ⁰C for ambient design temperature of 40 ⁰C.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.