{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the Quantum QUCM module and who supports it?
Issue: Support assistance


Product Line: Quantum


Environment: None


Cause: CAPP partner


Resolution:

Quantum Universal Communications Modules (QUCM+002, QUCM+102 & QUCM+204) are programmable serial communication modules for Schneider Automation's Quantum® PLC with two or more serial ports, a PLC interface, a LCD display with keypad, a real-time clock, a TCP/IP stack, and internal registers, made by Niobrara R&D. The QUCM+102 and QUCM+204 offers Ethernet port(s).

NR&D (Niobrara Research and Development).is Schneider Electric's Collaborative Alliance Partner.

QUCM modules can be ordered directly from them and is also supported by them.

Below is a link and phone number for ordering the part from them directly.

http://www.niobrara.com/index.html
(417) 624-8918 - phone

Schneider Electric Global