{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can you power up the ATV312 with an external 24VDC supply?
Issue:
ATV312 powered up with external 24VDC supply

Product Line:
Altivar 312, ATV312

Environment:
All

Cause:
3-phase power not available. There may be a need to program the drive before shipping it to an end customer, for example.

Resolution:
No, the ATV312 drives cannot be powered up using an external 24VDC power supply.