{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you change the display on the ATV312 drive to show motor current instead of motor frequency?
Issue:
ATV312 showing Motor current and not motor hz

Product Line:
Altivar ATV312

Environment:
All

Cause:
Changing main display to show different values.

Resolution:
Using the front display knob push enter.
Scroll down to the SUP menu and enter.
Scroll down to LCR (motor current) and enter.
While the current value is displayed (0), press and hold in the enter dial for 2seconds, display will flash once.  Motor current is now saved as default, even though a power cycle.

Schneider Electric Global