Issue:
Command switching is not visible on the ATV71.
Product Line:
Altivar 61, Altivar 71
Environment:
All serial numbers, all model numbers
Cause:
N/A
Resolution:
On the ATV61 or the ATV71, command switching will not be visible if profile is "not separate". Profile set to "not separate" means the command comes from the same place as the reference.
Command switching is not visible on the ATV71.
Product Line:
Altivar 61, Altivar 71
Environment:
All serial numbers, all model numbers
Cause:
N/A
Resolution:
On the ATV61 or the ATV71, command switching will not be visible if profile is "not separate". Profile set to "not separate" means the command comes from the same place as the reference.
Released for:Schneider Electric Global