{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can a file that is saved in the VW3A1101 LCD keypad be deleted?
Issue:
Saving and deleting a file in the VW3A1101 LCD Keypad.

Product Line:
ATV61 ATV71

Environment:
VW3A1101 keypad

Cause:
Existing files need to be removed to ensure they are never selected.

Resolution:
A file that is denoted as USED cannot be deleted back to the FREE status.  A USED file can be overwritten.
Suggestion is to SAVE AS multiple times to all USED files that need to be deleted.

Schneider Electric Global