Why the bluetooth interface TCSWAAC13FB does not restart after a power cut when is connected to the PLC TM221
Published date:
04 September 2018
As described in the Hardware Guide of SoMachine Basic, the PLC TM221xx RJ-45 connector with RS485 has some pins that MUST not be connected: Pins 1,2,3 and 6.
Please do not use 8 wires cables, use the cable reference XBTZ9980 (4 wires cable).
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.