Issue:
There doesn't appear to be a castor kit for the 6U, 9U or 12U NetShelter WX cabinets.
Product Line:
NetShelter WX
Environment:
All versions and serial ranges.
Cause:
There is a request to add castors to AR106, AR109, AR112, AR106SH4, AR109SH4, AR112SH4, AR106SH6, AR109SH6, AR112SH6, AR106V or AR106VI.
Resolution:
There is no castor kit for the AR106, AR109 or AR112.
The smallest cabinet that has a castor kit available is the AR100 and AR100HD. They use AR8359 available as a castor kit.
There doesn't appear to be a castor kit for the 6U, 9U or 12U NetShelter WX cabinets.
Product Line:
NetShelter WX
Environment:
All versions and serial ranges.
Cause:
There is a request to add castors to AR106, AR109, AR112, AR106SH4, AR109SH4, AR112SH4, AR106SH6, AR109SH6, AR112SH6, AR106V or AR106VI.
Resolution:
There is no castor kit for the AR106, AR109 or AR112.
The smallest cabinet that has a castor kit available is the AR100 and AR100HD. They use AR8359 available as a castor kit.
Released for:Schneider Electric Global